New Inject/Eject Solution Offers Hot Swap Function Protection

October 10, 2018 Rachel Pilgren-Kane

Southco has expanded its line of industry-recognized electronics solutions with a new P7 Inject/Eject Handle Set designed for full size AMC (Advanced Mezzanine Cards) carriers with hot swap function protection for AdvancedTCA® (ATCA) applications.

Southco’s new P7 Inject/Eject Handle Set is a complete solution including upper and lower latches and a switch arm, designed to mount to a faceplate accessible from the front of a system, allowing hot swap functionality. Hot swappable systems are crucial in managing the safety of stored data; if one system is down and running without a backup, the data is at risk until maintenance can restore redundancy.

Ejector systems like Southco’s P7 series provide the correct amount of “wipe” by ensuring that board connectors interface properly with the backplane of the shelf. When the P7 lever is released, a signal is sent by the integral micro-switch, which in turn releases that data successfully to a redundant line card, allowing the faulty card to be serviced or swapped out.

Southco is the leading supplier of front panel hardware with expertise in the functionality, flexibility, ergonomics and technicalities of PICMG standards affecting AdvancedTCA® (ATCA), AdvancedMC™ (AMC), and MicroTCA®. As a member of PICMG, Southco has developed a full range of products including ejector handles, alignment/keying blocks and captive retention screws in accordance with their standards.

For more information about our solutions for electronics, visit the Southco Resource Center-Electronics Page.

The post New Inject/Eject Solution Offers Hot Swap Function Protection appeared first on Southco Blog.

Previous Article
New Mini Cam Latch Designed for Limited Space Applications
New Mini Cam Latch Designed for Limited Space Applications

Southco has added to its broad range of cam latches with the introduction of the miniature E5 Cam Latch. Fe...

Next Article
New Compact Electronic Slide Bolt Designed For Small Spaces
New Compact Electronic Slide Bolt Designed For Small Spaces

Southco has expanded its line of electronic access control solutions with a compact electronic slide bolt t...