Southco Blog

Follow our blog for the latest product launch information and STEM events

  • New Inject/Eject Solution Offers Hot Swap Function Protection

    New Inject/Eject Solution Offers Hot Swap Function Protection

    Southco has expanded its line of industry-recognized electronics solutions with a new P7 Inject/Eject Handle Set designed for full size AMC (Advanced Mezzanine Cards) carriers with hot swap...

    Read Article
  • New Compact Electronic Slide Bolt Designed For Small Spaces

    New Compact Electronic Slide Bolt Designed For Small Spaces

    Southco has expanded its line of electronic access control solutions with a compact electronic slide bolt that simplifies the upgrade from mechanical to electromechanical latching. The lightweight...

    Read Article
  • Stainless Steel Rotary Latches Provide High Corrosion Resistance

    Stainless Steel Rotary Latches Provide High Corrosion Resistance

    Southco has expanded its line of rotary latches with a stainless steel version of the R4-20 Rotary Latch, which is designed with high corrosion-resistance for demanding Marine and Off-Highway...

    Read Article
  • Sealed Electronic Actuator Simplifies Upgrade from Mechanical Latching

    Sealed Electronic Actuator Simplifies Upgrade from Mechanical Latching

    Southco has recently added to its line of electronic actuators with a sealed version that simplifies the upgrade from mechanical to electronic actuation. Capable of accommodating higher mechanical...

    Read Article
  • New Cam Latch Offers Adjustable Grip For Custom Fit

    New Cam Latch Offers Adjustable Grip For Custom Fit

    Southco has expanded its successful E5 Cam Latch series with a new version that provides flexible grip adjustment, allowing a single latching solution to be used for multiple applications. Capable...

    Read Article
  • New Compact Actuator Enables Electronic Actuation of Mechanical Latches

    New Compact Actuator Enables Electronic Actuation of Mechanical Latches

    Southco has expanded its line of electronic access solutions with a compact electronic actuator that simplifies the upgrade from mechanical to electronic access. The AC-EM 05 Electronic Actuator...

    Read Article
  • Heavy-Duty Actuators Enable Actuation of Multiple Rotary Latches

    Heavy-Duty Actuators Enable Actuation of Multiple Rotary Latches

    Southco has further expanded its successful line of rotary latching solutions with the launch of two new heavy-duty, paddle-style actuators that provide multiple points of actuation, allowing two...

    Read Article
  • Heavy-Duty Two-Stage Latch Now Available in Stainless Steel

    Heavy-Duty Two-Stage Latch Now Available in Stainless Steel

    Southco’s has expanded its successful line of rotary latching solutions with the addition of a stainless steel version of its popular R4-30 series. Constructed of high-strength,...

    Read Article
  • RFID Access Controller Simplifies Electronic Access Control Set Up

    RFID Access Controller Simplifies Electronic Access Control Set Up

    Southco has expanded its line of electronic access solutions with an access controller that simplifies the integration of keyless access into equipment level applications. Southco’s EA-P3 High...

    Read Article
  • New Padlockable Cam Latch Features Redesigned Wing Knob

    New Padlockable Cam Latch Features Redesigned Wing Knob

    Southco has redesigned the wing knob version of its successful E5 Cam Latch series with a stylish, streamlined design that promotes improved ergonomics and enhanced security. The new E5 Wing Knob...

    Read Article
  • Bluetooth Controller Allows Smartphones To Be Used As Keys

    Bluetooth Controller Allows Smartphones To Be Used As Keys

    Southco has recently expanded its line of Electronic Access Solutions with an access controller that allows Bluetooth-enabled devices, such as smartphones and tablets, to be used as a key....

    Read Article
  • New Low Profile Captive Screw Designed For Tight Spaces

    New Low Profile Captive Screw Designed For Tight Spaces

    Southco has recently expanded its Captive Screw offering with a low profile version designed for applications where installation space is extremely limited. The 52 Miniature Captive Screw Low...

    Read Article
  • New Height Adjustable, Vertically Articulating Arms

    New Height Adjustable, Vertically Articulating Arms

    Southco has expanded its AV Display Mount offering with two new versions that allow the height of a monitor or display to be precisely adjusted according to end user preferences. The expanded...

    Read Article
  • Rotary Latch Features Integrated Cable Mounting Bracket

    Rotary Latch Features Integrated Cable Mounting Bracket

    Southco has recently expanded its successful line of rotary latching solutions with the launch of the R4-10 Rotary Latch with Integrated Bracket. The newest addition to the R4-10 Rotary Latch...

    Read Article
  • New Cable Splitter Provides Timed Release Of Rotary Latches

    New Cable Splitter Provides Timed Release Of Rotary Latches

    Southco’s newest addition to its successful line of Rotary Latch solutions allows multiple connected rotary latches to be triggered from a single actuation point. The AC Cable Splitter features...

    Read Article
  • Rotary Latch Features Direct, Cable-free Actuation

    Rotary Latch Features Direct, Cable-free Actuation

    Southco’s newest rotary latch can be triggered directly via push button or lever-style actuator, without the need for connected cable or rod. A rubber covered trigger alleviates potential noise...

    Read Article
  • Padlockable Compression Latch Offers Enhanced Security

    Padlockable Compression Latch Offers Enhanced Security

    Southco has expanded its successful E3 VISE ACTION® Compression Latch series with an ergonomic T-handle version that features an integrated padlockable design. The padlockable E3 VISE ACTION®...

    Read Article
  • Southco Apprentice Wins Best of British Engineering Award From Semta

    Southco Apprentice Wins Best of British Engineering Award From Semta

    Southco apprentice Philippa Dressler-Pearson was recently awarded the UK Apprentice of the Year and Best of British Engineering at the Semta Skills Awards ceremony in London, UK. Semta (The...

    Read Article
  • New Counterbalance System Neutralizes Weight of Heavy Doors and Covers

    New Counterbalance System Neutralizes Weight of Heavy Doors and Covers

    Southco has recently expanded its Positioning Technology portfolio with the addition a system designed to neutralize the weight of heavy doors and covers. The CB Lift-A-SYST® series combines...

    Read Article
  • Countering the Threat of Physical Security Breaches in Colocation Centers

    Countering the Threat of Physical Security Breaches in Colocation Centers

    In today’s world, data is fast becoming the new global currency and as data volumes continue to grow at an exponential rate, the issue of data security continues to cause concern within the...

    Read Article
  • loading
    Loading More...