Rachel Pilgren-Kane

  • New Mini Slide Latch Meets Limited Space Requirements

    New Mini Slide Latch Meets Limited Space Requirements

    Southco has expanded its line of A3 Slide Latches with a new version that is 35% shorter than Southco’s smallest A3 product series, providing reliable performance for applications where space is...

    Read Article
  • Plastic Constant Torque Hinge Provides Customized Operation and Resists Corrosion

    Plastic Constant Torque Hinge Provides Customized Operation and Resists Corrosion

    Southco has expanded its successful line of E6 Constant Torque Hinges with a plastic version designed for use in corrosive environments. Southco’s line of Constant Torque Position Control Hinges...

    Read Article
  • New Steel Rotary Latch Features Hand Actuation

    New Steel Rotary Latch Features Hand Actuation

    Southco has expanded its line of rotary latches with a new version that can be triggered by hand via an integrated plastic knob, eliminating the need for a separate cable and actuator. The hand...

    Read Article
  • New Mini Cam Latch Designed for Limited Space Applications

    New Mini Cam Latch Designed for Limited Space Applications

    Southco has added to its broad range of cam latches with the introduction of the miniature E5 Cam Latch. Featuring a 30% reduction in intrusion compared to Southco’s standard E5 Cam Latch series,...

    Read Article
  • DZUS® Quick Access Fastening Solutions Brochure

    DZUS® Quick Access Fastening Solutions Brochure

    This brochure explains important design considerations for specifying a DZUS® Quick Access Fastener and offers a step-by-step guide to selecting a complete fastening system from Southco.

    Read Flipbook
  • New Inject/Eject Solution Offers Hot Swap Function Protection

    New Inject/Eject Solution Offers Hot Swap Function Protection

    Southco has expanded its line of industry-recognized electronics solutions with a new P7 Inject/Eject Handle Set designed for full size AMC (Advanced Mezzanine Cards) carriers with hot swap...

    Read Article
  • New Compact Electronic Slide Bolt Designed For Small Spaces

    New Compact Electronic Slide Bolt Designed For Small Spaces

    Southco has expanded its line of electronic access control solutions with a compact electronic slide bolt that simplifies the upgrade from mechanical to electromechanical latching. The lightweight...

    Read Article
  • Stainless Steel Rotary Latches Provide High Corrosion Resistance

    Stainless Steel Rotary Latches Provide High Corrosion Resistance

    Southco has expanded its line of rotary latches with a stainless steel version of the R4-20 Rotary Latch, which is designed with high corrosion-resistance for demanding Marine and Off-Highway...

    Read Article
  • New Recognition Certification for Access Hardware Components Used in Electrical Enclosures

    New Recognition Certification for Access Hardware Components Used in Electrical Enclosures

    This article explains how enclosure manufacturers can can save time and money on corrosion testing with UL recognizes access hardware products from Southco.

    Read Article
  • Sealed Electronic Actuator Simplifies Upgrade from Mechanical Latching

    Sealed Electronic Actuator Simplifies Upgrade from Mechanical Latching

    Southco has recently added to its line of electronic actuators with a sealed version that simplifies the upgrade from mechanical to electronic actuation. Capable of accommodating higher mechanical...

    Read Article
  • Southco EA-BT BLUETOOTH® Controller Earns 2018 Money-Saving Product Award

    Southco EA-BT BLUETOOTH® Controller Earns 2018 Money-Saving Product Award

    Southco’s EA-BT BLUETOOTH® Controller is a BUILDINGS Magazine 2018 Money-Saving Product winner.

    Read Article
  • New Cam Latch Offers Adjustable Grip For Custom Fit

    New Cam Latch Offers Adjustable Grip For Custom Fit

    Southco has expanded its successful E5 Cam Latch series with a new version that provides flexible grip adjustment, allowing a single latching solution to be used for multiple applications. Capable...

    Read Article
  • Southco Expands Europe Manufacturing Operations Into Poland

    Southco Expands Europe Manufacturing Operations Into Poland

    Southco has announced that it will expand its operations footprint into Rzeszów, Poland to meet the needs of the company’s growing European customer base.

    Read Article
  • New Compact Actuator Enables Electronic Actuation of Mechanical Latches

    New Compact Actuator Enables Electronic Actuation of Mechanical Latches

    Southco has expanded its line of electronic access solutions with a compact electronic actuator that simplifies the upgrade from mechanical to electronic access. The AC-EM 05 Electronic Actuator...

    Read Article
  • Geven & Southco: Taking the Load Off Aircraft Seating with Innovative Hinge Technology

    Geven & Southco: Taking the Load Off Aircraft Seating with Innovative Hinge Technology

    This case study explains how Southco helped Geven enhance the functionality and reliability of their passenger seat headrest design with a lightweight, constant torque hinge solution.

    Read Flipbook
  • Heavy-Duty Actuators Enable Actuation of Multiple Rotary Latches

    Heavy-Duty Actuators Enable Actuation of Multiple Rotary Latches

    Southco has further expanded its successful line of rotary latching solutions with the launch of two new heavy-duty, paddle-style actuators that provide multiple points of actuation, allowing two...

    Read Article
  • Heavy-Duty Two-Stage Latch Now Available in Stainless Steel

    Heavy-Duty Two-Stage Latch Now Available in Stainless Steel

    Southco’s has expanded its successful line of rotary latching solutions with the addition of a stainless steel version of its popular R4-30 series. Constructed of high-strength,...

    Read Article
  • More Autonomy in the Near Future for Off-Highway Equipment

    More Autonomy in the Near Future for Off-Highway Equipment

    Read Article
  • How Southco Is Using Technology To Connect To Industry 4.0

    How Southco Is Using Technology To Connect To Industry 4.0

    This article explains how Southco is transforming its facilities into “smart” factories by connecting software with processes to increase efficiency while reducing defects, downtime and waste.

    Read Article
  • Safeguarding the Success of Industrial Products

    Safeguarding the Success of Industrial Products

    This article explains how manufacturers can meet their operational goals with proven access hardware solutions that address key issues around design, safety, efficiency, performance and flexibility.

    Read Article
  • loading
    Loading More...